• AD5624

    Can someone clarify where in the data sheet for this device (section Software Reset) where the command 110 is defined as software reset. Elsewhere in Table 7 Reset is defined as 101 and LDAC Register load is defined as 110.

    Many thanks

    Mike

  • AD5624 Command 010 doesn't work

    Dear Sirs,

    We have a customer which is evaluating nano DAC AD5624. The engineer told that a command 010 which is reserved to Write to input register n and update all DACs(software LDAC) doesn't work properly.

    if the engineer writes and update each…

  • RE: Exposed Pad in AD5664/AD5624

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • different voltages for vcc and vref for AD5624?

    Can the vdd and vref of AD5624 be of different voltages?.Like vcc/vdd be 3.3V and Vref be 5v.so that there is no need  for a volatge level shifter for the ic from 3.3v to 5v.

  • Is AD5624 a possible replacement for AD5324?

    We are looking at alternates for the AD5324 (mainly for cost reduction), and it seems that the AD5624 is a good candidate. Would the AD5624 be considered a very close replacement for the AD5324? The current DAC is used in a low speed correction loop with…

  • RE: ADL5375 noise floor

    Hi Dragan,

    You're welcome. Good to hear you were able to troubleshoot it to the baseband common mode voltages.

    In terms of baseband interface, the following are possibilities you might consider:

    1. Use differential output transmit DAC with common mode…
  • 2011-01-19 06:02:35     Query regd ad5624r_spi.c operation. Is it jitter free?

    2011-01-19 06:02:35     Query regd ad5624r_spi.c operation. Is it jitter free?

    Ashish Gupta (INDIA)

    Message: 97550   

    Hi,

    We have a custom BF527 based processor platform and are curerntly selecting suiatble DAC chips for interfacing with Blackfin. We…

  • RE: Are there non-reference options available of the AD5664R and the AD5624R?

    Yes, The AD5624 and AD5664 are the non-reference options of the AD5624R and AD5664R.

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • RE: nanoDAC-What are nanoDACs?

    nanoDACs are a portfolio of products which combine small package, low power and low cost digital to analog conversion.

    nanoDACs are monotonic DACs which can be powered off a single 3V or 5V supply and are available in the industries smallest packages…