• RE: AD5620 as amplitude control AD9834

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • zero code error and offset error of AD5620

    I am using AD5620, the expected Vout should be 0.8V according to the equation: Vout = 2 x Vrefout x (D/2^N), where D=1310, but I measured the Vout is around 0.84-0.85V. And I measured the zero code error is around 0.3V.

     I checked the datasheet where…

  • RE: 关于AD9834和AD5620输出的方波幅值可调的问题

    This question has been closed by the EZ team and is assumed answered.
  • RE: AD5620 or AD5640- Using Vfb to control the DAC output

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: 关于AD9834和AD5620输出方波幅值可调与否的问题

    This question has been closed by the EZ team and is assumed answered.
  • RE: the adjustable amplitude of square wave generated by AD9834 and AD5620

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD5620 Serial Interface Problem

    Hi

    I'm using a AD5620 nana-DAC part. I have an intermittent failure. Sometimes the part does not respond to serial interface commands. The voltages remains at 0V even though I'm sending serial commands to it. If I cycle the power to the device, the problem…

  • Low Ref on AD5620. Why?

    Hello

    I measure voltage level on Vref pin. He is +2,483V. I changed supply voltage from + 5V to + 6V. Vref is const.

    In the datasheet specified tolerances Vref from +2,495V to +2,505V.

    Why value on an output is other than declared in datasheet?

  • AD5620 Model Options

    i have a question about AD5620 Model Options.

    what difference between AD5620A..., AD5620B... and AD5620C...? Difference is only in relative accuracy between models (A the best?)

    next, AD5620-2-3 parts include an internal, 2.5 V, 5 ppm/°C reference,…

  • EVAL-AD5662/AD5660/AD5640/AD5620

    Hi everyone!

    I'm using EVAL-AD5662/AD5660/AD5640/AD5620 and have AD5660 as my DAC and I noticed that there are grounding problems to the AGND and DGND pins of the evaluation board. It is said in the datasheet of the evaluation board that the analog GND…