• AD5602 command list

    I was going through the AD5602 datasheet and could not find any registers map or commands list to talk to DAC.

    1. How to read the ad5602 chip status?
    2. How to perform software reset?
    3. How to instruct to generate output?

    Any information will be useful to move…

  • I2C clock stretching on DAC products

    Hi,

     

    We are checking if AD5602 and AD5242 are having I2C optional clock stretching function embedded in SCL pin. Could you please make sure ?

     

    If they are not, please help us to find any other ADI DAC and DigiPot products having this feature ?

     

  • RE: AD5760 Supply Range

    Hi!

    The application is a precision power supply, that would ideally be able to replicate low-frequency signals (A few KHz) but that's not a strict requirement for the device. The output voltage is 0-25 V. I've realized that I was being a bit silly about…

  • RE: nanoDAC-What are nanoDACs?

    nanoDACs are a portfolio of products which combine small package, low power and low cost digital to analog conversion.

    nanoDACs are monotonic DACs which can be powered off a single 3V or 5V supply and are available in the industries smallest packages…

  • nanoDAC - Which DACs should be used for open loop systems and which DACs should be used in closed loop systems?

    It must be stressed that depending on the application performance requirements, all nanoDACs can be used in both open and closed loop systems.

    In an open loop application the DAC drives the load (a valve or an actuator, for example) directly while in…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…