• AD5592R Registers

    Hi, 

    I'm assessing whether AD5592R could be used in an airborne unit, for SEU immune purpose, I was wondering are the registers of AD5592R flash-based or RAM-based?

    Thank you very much,

    Cloud 

  • RE: Register read back is not working in the AD5592R.

    Hi

    Have you verified the timing pattern against the one in the datasheet on the oscilloscope.

  • AD5592R

    AD5592R/AD5592R-1 FAQ

     

    Q1. What is the difference between the AD5592R and AD5592R-1?

    A1. The operation and performance of the DACs, ADCs and GPOIs in the AD5592R and AD5592R-1 is identical. The AD5592R is a true single supply device. There is one…

  • AD5592R

    Hello,

    I am using an AD5592R DAC but having trouble running the code. I have taken and tried both the C and Python scripts from your website but getting a response from the SPI is proving difficult. Any support or examples you could provide would be greatly…

  • AD5592R read volt

    HI team:

        Now I use the AD5592R chip to cycle read the voltage. I find that when I set all channels of the ADC Pin Configuration Register to 1 and only one channel of the ADC sequence register is configured for conversion, the result of ADC conversion…

  • RE: EVAL-AD5592R ADC/DAC combination

    Conversion time is 2us max. Sampling time is 500ns min. So the total time required by ADC is 2.5us min .. Hence the conversion or throughput rate is 400kSPS.

  • AD5592R DAC output limit

    Pretty much know the answer, but I’ll ask anyway since the datasheet implies otherwise.

    First use of the AD5592R with one DAC output, two A/D inputs, and one GPIO used.

    Operating it at 3.3v since the SPI I/O coming from SN65LVDT41/14 LVDS SPI datalink…

  • AD5592R驱动

    请问有没有基于stm32的AD5592R的驱动代码??现在写的驱动数据收发不正常!!

  • Question about ad5592r DAC output

    Hello,

    we are using Arduino UNO to control AD5592R, output a range of voltages. 

    We want to know how long it takes the DAC to set and achieve its output voltage.

    #include <libad5592r.h>
    ad5592r_t ad5592r;
    
    const int pin = PB0;
    
    void setup() {
      /…

  • AD5592R analog input/output range

    Hi,

    I'm a bit confused about the analog input/output range of the AD5592R.

    If I set Vref = 5V, and configure the ADC/DAC to 2xVref mode (set D4 and D5 of the general-purpose control register to 1), does it mean the chip is able to receive and output…