• AD5590

    Does anyone have a driver for the AD5590? 
    Is it possible to get the source code for the firmware on the eval board?

  • Using AD5590 with Arduino

    I am trying to use the AD5590 with an Adafruit ESP32 Feather and the Arduino IDE.  As a starting point, I have connected the ESP32 to the AD5590 evaluation board and I am trying to get the DACs to work. However, I unable to get a response from the DACs…

  • AD5590 with 3.3V MCU

    I have written a driver for the AD5590 and tested it with the Arduino Uno. My code works correctly on the Uno which is a 5V system. I am now trying to make the code work with a 3.3V ESP32. With the ESP32, the ADCs return values that are double what they…

  • ad5590

    Hi,

    i am trying to read the dac out 0 using adc0 (ad5590ebz) what should be the jumper configuration for this? is any external power supply required other than usb in . i am trying monitor the adc out using evk software i am not getting any out put!!…

  • AD5590 ADC count not consistant

    Hi,

    I am using AD5590 ADC in my design for voltage and current measurement. using all 16 channels.
    Below is the Configuration that I followed. Following the sequence as provided.
    2Cycles of dummy write with ADIN High.

    (0xffff);        //Dummy Write
    (0xffff);        //Dummy…

  • Control of AD5590 with one of the SPI bus of a Raspberry

    Hello,

    We are using the AD5590 both for its capabilities of DAC and ADC.

    We are able to control the DAC with the Raspberry SPI0 bus by linking SCLK, MOSI, CE0 and CE1 (Raspberry) to the AD5590 pins, DSCLK, DDIN and DSYNCK1 and DSYNCK2 respectively.

    We…

  • AD5590 GUI

    I would like to control the AD5590 using an external program (e.g. Labview).

    Is it possible to have a copy of the source code for this device?

    Thanks for your time and help

    Best Regards

    Ian

  • RE: AD Evaluation Boards used in C# - ADI-CYUSB_USB4.dll

    Hi suiraM, jlala,

    I was wondering if anybody could provide example code to read/write the AD5590 ADC/DAC?

    Thanks in advance

    Best Regards

    Ian

  • RE: Measurement of pulse amplitude - suggestion for ADC

    Hi Henning,

         We have some I2C ADC interface that may fit your application, you may check the AD799x. Just like to ask on when are going to use the trigger feature, is it when the pulse amplitude hit some kind of limit or outside the range? I am also…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…