• 为什么AD5560芯片没有"FI"功能

    为什么AD5560芯片没有"FI"功能呢?是没有设计还是出于什么考虑?

  • AD5560's Clamp Enable Input status.

    What is the status, high or low, of AD5560's Clamp Enable Input Pin( Pin No. is 14), when it floating(open)?

    I want to control the clamp enable(high) or disable(low) using by on/off switching.

  • RE: Why does  AD5560  not have "FI" function?

    Hi Alan,

      So in FI mode, does the clamp function as voltage clamp then. How to set the voltage clamp?

  • RE: AD5560 MEASOUT in Voltage mode drift

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD5560 package issue vs Temperature

    1.Temperarture scals issue with different package

    2.Pin1 issue

    Dear  ADI,

    We are now designing AD5560. For the package issue, we are confused about BGA and TQFP.

    As we read from datasheet, we think 3 hot points are shown in the BGA package. But the…

  • There are terrible noise (sine wave) on the AD5560 FORCE OUTPUT while operating

    Hello , mates

    I have a strange terrible problem when operating my AD5560 board. Eight AD5560s are powered by a common -5V power rail ( LTM8027 )  , and each chip's HCAVDD powered by 10.5V  independently generated from LTM4622A . 

    Now when I force voltage…

  • AD5560 DUTGND voltage range

    Hi, 

    DUTGND voltage range is specified -1V to +1V in Table1.

    When exceeding this voltage range with pull-up function disabled, is DUTGND clamped internally +1V or -1V?

    I would like to know whether AD5560 work normally or not when DUTGND exceeding the…

  • Questions about AD5560 SPI and voltage forcing

    Hi,

    I've met problems on using AD5560 with Arduino.

    1.My force pin output give ground value after I set the DAC.

    2.My register SPI readback doesn't match desired value.

    Only basic functioning pins were connected: SPI, power and grounds, force&sense…

  • Questions about GUI & parameters of AD5560 EVM Software

    Hello,

    My customer is trying to confirm the performance of AD5560 using ADI EVM.

    For this, they want to measure current values as changing voltage values.

    As changing voltage values, they will add additional load to be measured pin.

    For doing above…

  • AD5560 Force Current Limit issue

    Hello!!

    I am now testing the AD5560 Eval Borad. An external load is connected and test the output of the current. A current of about 300 mA  more is not output(less than 300mA Current output OK). The current clamp is not used and the measured value is…