• AD5545, error in data sheet?

    In the data sheet for AD5545/AD5555 (rev. I), in the figure 22, there is a voltage regulator ADR03 connected by VIN to VREF of AD5545/AD5555. Is it an error? Or, maybe, there is some sense in this connection?

    And, BTW, another question about this scheme…

  • AD5545 Dual DAC using shared reference

    Hi,

    I would like to use one reference for both DACs of the AD5545. My question is if it would be suitable to connect both reference pins (VrefA and VrefB) to the output of the reference without using switches in the two lines. Attached is a snippet of…

  • RE: PROBLEM-AD5545 AMPLITUDE DECREASING AT HIGHER FREQUENCY

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD5545 HDL code AVAILABLE?

    i wanna macke DAC DESIGN in VERTEX-7 for AD5545 could u help me for this 

  • RE: [征文+原创] 电流输出型DA转换器AD5545的原理,应用及编程

    This question has been closed by the EZ team and is assumed answered.
  • ads1672 adc to AD5545 DAC loopback in fpga 

    hai every one,

    i wanna  make ADC (ads1672) output 24 bit data to DAC (AD5545) 16 bit input. 

    how could i make loop back between 2. 

  • RE: [征文+原创] 电流输出型DA转换器AD5545的原理,应用及编程2

    This question has been closed by the EZ team and is assumed answered.
  • Ibis model for AD5545

    Hi, All

    I can not find the IBIS model of the AD5545 also look at the web site.

    Can you provide a simulation model for AD5545?

    Best Regards,

    Laliberte

  • About Input Resistance (Rref) of AD5545

    Hi, All.

    I am a design using the AD5545.

    Datasheet there a specification of the typical value as Input Resistance (Rref) in the "REFERENCE INPUT Parameters", but please tell us about the max / min values.

    Best Regards,
    Laliberte

  • Hai ,Can any one suggest an ic to generate negative reference voltage for AD5545 to get positive o/p voltage from DAC of range 0 to 5V

    Hai ,Can any one suggest an ic to generate negative reference voltage for AD5545 to get positive o/p voltage from DAC of range 0 to 5V.