Assumed this query has been closed.
Hello all,
I am planning to make a programmable current source using this circuitry, so can I put 100mV at V_reference externally on this IC to generate properly.
In the datasheet though the entire range is given but can we give 100mV at the Vin that…
Hello everyone:
There is a qusetion about 16 Bits DAC AD5543.It is described that "The PCB metal traces between VREF and RFB must also be matched to minimize gain error"in the data sheet. So,how to do it?What should i do to make them matched…
I'm planing to use an AC signal (10Vp-p without DC bias) as Vref. But haven't seen any doc mentioned this. The most similar one is "Multiplying DACs—AC-Arbitrary Reference Applications", but the 'AC references' mentioned in it's examples are all…
我打算使用10V峰峰值的交流信号做AD5543的基准。但是目前找到的ADI的所有资料都是使用的正电平(即使是正弦波也是加了正偏置的)做其基准。所以想确认下,能不能用无偏置的正弦信号做其基准,如果可以,与固定电平基准配置相比,要额外注意些什么?