• EVAL-AD5541A/42ASDZ connection issue

    Hello,

    I have bought EVAL-AD5541A/42ASDZ and find out cannot connect to computer to evaluate.

    Is that EVAL-SDP-CB1Z is the missing part i needed to order?

    Do EVAL-SDP-CB1Z come with a necessary cable that i can connect to U10 of EVAL-AD5541A/42ASDZ…

  • Where do I tie the exposed paddle on DACs such as the AD5541A, AD5542A, AD5512A, AD5668, AD5628, AD5669 and AD5629 that are packaged in LFCSP?

    Where do I tie the exposed paddle on DACs such as the AD5541A, AD5542A, AD5512A, AD5668, AD5628, AD5669 and AD5629 that are packaged in LFCSP?

  • Which reference should be used with the AD5541A/42A?

    Which reference should I choose to get the best performance from the AD5541A/42A?

  • AD5541A output range

    Hello,

    I'd like to supply 5.00 V to both Vref and Vdd on a AD5541A DAC. According to the datasheet, this is ok.  It's convenient because the DAC's current draw is low and it will save a voltage regulator.  What will the output voltage range…

  • RE: SDP-B + EVAL-AD5541ASDZ

    Hello Masaki,

    The easiest way to do this is to modify the program that controls the AD5541A via the SDP. The program is written in labview so if you have that I can send you the source code.

    If not, I can make the changes for you.

  • AD5541A glitches every 512 codes

    The AD5541A on our board is producing noise glitches at 512-code intervals.  To be specific, when stepped in increments of 32 DAC codes, starting at mid range (0x8000), we see noise glitches every 16 increments (e.g., at 0x8200, 0x8400, etc.).  I might…

  • AD5791 operate voltage

    Hello, 

      I have use AD5541A ( 16 bit DAC ) for a while and have very good use experience with AD5541A.

      now I hope to try their family which is enhance to 18  or 20 bit DAC, that is  AD5791. 

      unfortunately AD5791's positive reference voltage  is recommend…

  • RE: Op amp to drive 10uF capacitor

    Hi James,

    I am the applications engineer supporting the AD5541A. I can't recommend a suitable amplifier, (though someone on this forum should be able to) but I can give some pointers.

    The AD5541A is an R-2R DAC architecture, which means that when…