• Scripting control of the AD5535B Evaluation Board

    Hi -- I am hoping to control the AD5535B Evaluation Board using some kind of software scripting (Python preferred). I have the SDP-S Controller Board and can run the sample GUI, but I haven't been able to find much in the way of drivers or an API to allow…

  • A problem about AD5535B voltage output

    I Connect the 60 V power supply to EVAL-AD5535BSDZ's VPP and connect the 5 V  supply to AVCC, DVCC, and V+ (5 V). But the  measured value of VOUT is not the calculated value based formula of datasheet of AD5535B.  The formula is .

  • EVAL-AD5535B with SDP-S USB com board

    The provided software, written in LabView, can only update one channel per update.

    Out controllable optics requires multiple channel updates at a fairly high rate, ~1 khz.

    Is there a LabView software for this EVAL board capable of affecting multi-channel…

  • 关于AD5535B电压输出问题

    1. 我将60V直流电压接到评估版EVAL-AD5535BSDZ的Vpp,将5V直流电压接到AVcc、DVcc、和V+,将他们的地AGND、DGND短接,然后将评估版与电脑连接,设置参考电压1.024V,输入代码,测量输出电压(V0-V31),发现测量值与公式 计算值对不上,这是怎么回事?

    2. 测量输出电压是不是以AGND或DGND作为参考地?

    3. 如果公式计算值与实际测量值确实对不上,我怎么根据需要的电压设置相应的代码?

  • AD5535B using all channels together

    Hi, I need an ADC for 200V but only one output.

    1. Adding output currents

    On the AD5535B each channel can drive: 550 µA, I wonder if is possible to use all together to supply more current? 0.55uA*32 = 17.6mA. I know that 550uA is the maximum, not reco…

  • RE: AD5535B driven capacity

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Differences between AD5535 and AD5535B

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD5535B channel-to-channel offsets and calibration?

    Working on a custom board with several AD5535B's driving an array of devices for testing, driving the chip in the 0-50V range (VREF=1.0 V).  With the chip in power-on-reset state and all channels zeroed, I observe a steady-state DC output voltage of…

  • Prototyping with the AD5535B EVAL board

    I am using an EVAL-AD5535BSDZ evaluation board to play with the AD5535 chip. I can use the provided software (through an SDP-S module).

    First off: I have heard people mention LabVIEW examples but cannot find them anywhere. Can anyone help me with this…

  • Example code for controlling the AD5535B

    Hi, I am using the AD5535BSDZ Eval Board with the SDP-CS1Z USB interface. I am able to set channel voltages using the provided evaluation software. Now I would like to send a squarewave (or other waveform) signal to the AD5535B. All the example code available…