• AD5520 STROBING

    I have a question about AD5520.
    My customers are considering AD 5520.
    My customers are not going to use comparator outputs (CPOH, CPOL).

    They plan to set digital inputs and then apply analog inputs (CLH, CLL, FIN).
    Experiment with the evaluation board, it…

  • AD5520的STANDBY模式

    这是AD5520数据手册里的话,意思是在改变操作模式或者改变量程的时候需要先进入STANDBY模式,这样可以避免放大器进入饱和区,就可以避免85微秒的恢复时间。而根据数据手册里面的时序图我们可以总结出完成一次测试需要1微秒左右,那么这个85微妙的恢复期就显得很长,严重影响

    测试速度。

    而数据手册里对STANDBY模式没有详细描述,具体描述如下:

    我的问题如下:

    1、STANDBY模式按照图1来说应该是必须的,那么没有这个模式在测试时会严重影响速度吗?

    2、STANDBY信号需要维持多长时间才能起作用…

  • AD5520:trouble with MEASOUT voltage range

    HI this is my sch of ad5520. the pin 64(CLL) vee_3v3 is -3.3V and pin 63(CLH) vcc_3v3 is +3.3v.

    I change the pin 26(FIN) voltage , the pin 58 (MEASOUT) should from -3.3V to + 3.3V . but the pin 58 (MEASOUT)  is -0.256V to 3.3V.

    the R74 is 100K. and…

  • RE: 这11大应用领域,你在里面么?

    仪表仪器和测量

    ADI我比较关注测试测量的。个人爱好。记得有一款AD5520适用于ATE设备的测试IC,per pin的PMU芯片,可能有点老了。官网有一块这个芯片的开发板可以做一些FVMI,FIMV等测试测量的实验,一直想玩一玩,奈何好贵啊,几千块了 。仅芯片就400+了 .不过还是很佩服ADI的。学到很多东西

  • What is a Source Measurement Unit or SMU?

    As more background on this last blog entry on measuring current with the ADALM1000 I thought it might be good to answer the question, What is a Source Measurement Unit anyway?


    A Source Measure Unit (SMU) is an instrument that combines a sourcing function…

  • TAGS LIST: Amplifiers

    AD600
    AD602
    AD603
    AD604
    AD605
    AD8264
    AD8330
    AD8331
    AD8332
    AD8334
    AD8335
    AD8336
    AD8337
    AD8338
    ADL5246
    ADL5330
    ADL5331
    LTC6412
    HMC6187G
    HMC997G
    HMC996
    HMC694G
    AD8368
    AD8351
    AD8367
    AD75071
    AD552…