Where do I tie the exposed paddle on DACs such as the AD5541A, AD5542A, AD5512A, AD5668, AD5628, AD5669 and AD5629 that are packaged in LFCSP?
你好,我看AD8628的文档说AD8628是单电源供电,但是在AD5512A的文档里,说AD5512A的双极性输出操作是,给出的例子里用的就是AD8628,但是图里面是接的确实双电源,如下图
我使用的AD5512A的双极性输出,那应该是5v单电源,还是双电源+-5V?谢谢
您好。DAC更新速度会受到建立时间,和通讯速度,以及其他一些时序要求的影响。
对于您的应用可以参考使用DDS产生正弦信号,可以参考AD9837。希望使用DAC的话,可以参考AD5512A,AD5552
I or V out可以参考AD5450,是电流输出的DAC,在Voltage-Switching Mode连接时可以做电压输出
unbuffered vout和voltage out输出阻抗不同
应用笔记* AN-764:用做匹配的ADF7020 RF端口阻抗值
* AN-771:ADSP-BF533 EZ-KIT Lite与ADF70xx接口
* AN-917:配合EVAL-ADF7020和EVAL-ADF7025评估板在868 MHz和915 MHz频率下使用LC谐波滤波器
* AN-920:利用AD9788 TxDAC和ADL5372正交调制器实现单边带发射机中的增益、LO和相位补偿
*
AN-922:数字脉冲整形滤波器基础知识
* AN-0982:残余相位…
AD5398, 120mA Current sinking DAC With Reduced Current Range
I'm working with the AD5398. I don't need the full 120mA range of the device. Is it possible to get the full 10bit resolution over a smaller current range, say 20mA? What would be the…