• AD5439: crosstalk problem

    We use AD5439 in a signal generator. We found crosstalk between the two
    channels when using the part. However, there is no crosstalk spec in the
    datasheet .Would you please give some suggestion to this problem.

     

    A table of crosstalk…
  • RE: Combining two DAC to double resolution (AD5439 or ?)

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: HMC812 Eval kit information

    FormerMember
    FormerMember

    Hi Sai,

    Attached is the PCB layout and gerber files for the HMC812LC4 Evaluation Board. This is a simple EVB circuit, we do not have the user guide or schematic diagram. The layout follows the same application circuit as shown in the HMC812LC4 datasheet…

  • RE: Issue with SPORT0 Receive Logic

    Prashant:

      I have a new issue with the SPORT0 Transmitter When I am trying to interface to the AD5439 Serial Dacs.  I can get the transmitter to send multiple frames, but only get one frame sync for the whole transmission, even while putting in a firmware…

  • Daisy chain issue with AD5415

    If you are using or plan to use the AD5415 12-bit DAC chip in a daisy-chain configuration, you need to read page 20 of the marked up data sheet attached.  If you are using the SDO output of even a single AD5415, then you also need to see the erratum marked…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…