Hello,
I would like to use AD5433 with unipolar mode.
And, I use R1 and R2 resistors to adjust the gain.
Please inform me of the expression that calculates this resistors.
Best Regards,
Mr.K
Hi,
Please use AD5445, the data also applies to AD5433.
Cheers,
Ivan
Hi cklooi,
Both DAC10BX and DAC10BX/833 are obsolete.
AD5433 (single) and AD5440 (dual) are 10-bit MDACs that could be offered as replacements, not pin for pin but with similar functionality.
Regards,
Estibaliz
AD693 |
AD5410 |
AD5412 |
AD5420 |
AD5422 |
AD5735 |
AD5755 |
AD5755-1 |
AD5737 |
AD5757 |
AD5421 |
AD421 |
AD5758 |
AD7569 |
AD7669 |
AD7868 |
AD7869 |
AD5593R |
AD5592R |
AD5940 |
AD5941 |
AD7293 |
AD7294-2 |
AD7292 |
AD5590 |
AD7294 |
L… |
AD5398, 120mA Current sinking DAC With Reduced Current Range
I'm working with the AD5398. I don't need the full 120mA range of the device. Is it possible to get the full 10bit resolution over a smaller current range, say 20mA? What would be the…
If you are using or plan to use the AD5415 12-bit DAC chip in a daisy-chain configuration, you need to read page 20 of the marked up data sheet attached. If you are using the SDO output of even a single AD5415, then you also need to see the erratum marked…