• AD5424: How to calculator R1 and R2 value?

    Hi,

    I designed a application use AD5424 and Op Amps UA741CDT with Vref =+5V, C1=1pF in below.

    I want the voltage of the Vout from 0V to -5V. How to calculator value R1 and R2 ? 

    P/s: I try to use R2 and R1=0 ohm but the Vout =1.9V and the Vout don't change…

  • RE: Replace an AD7524 by an AD5424.

    This question has been closed by the EZ team and is assumed answered.
  • Spikes on output of AD5424

    I am using your AD5424 DAC as a gain control between two OpAmps.  When I manually step the gain it works very well, but when I slew the DAC, incrementing one bit every 10uS, spikes appear on the output of the DAC when multiple bits are changing state. 

  • AD5424和AD8664的使用问题

    我在使用AD5424做幅值转换电路的时候,VREF端接入的是一个1KHz的正弦信号,可是无论怎么改变DB0-DB7,在AD8664的输出端总是+5V?电路图如下:

  • RE: Wiring examples for AD7524

    Hi Mats,

    There is an alternative circuit, the voltage switching mode, not using negative voltages. Although it is an existing option, we cannot garantee a good performance of the part as there is no characterization data for this configuration.

    VIN…

  • ADI中文技术论坛:专家解答热帖(2014年4月汇总)

    非常见问题解答——可调整或可编程的模拟输入范围有何优势?

    http://ezchina.analog.com/message/15833#15833

    AD-FMCOMMS3-EBZ  RF工程师平台”

    http://ezchina.analog.com/message/15743#15743

    ADV7604BBCZ-5 部分HDMI信号无法正常采集

    http://ezchina.analog.com/message/15514#15514

    AD-FMComms2-EBZ硬件评估板

  • RE: 超声成像

     PDF

    ADI提供了相关解决方案,具体请看附件。

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • Daisy chain issue with AD5415

    If you are using or plan to use the AD5415 12-bit DAC chip in a daisy-chain configuration, you need to read page 20 of the marked up data sheet attached.  If you are using the SDO output of even a single AD5415, then you also need to see the erratum marked…