• FAQ: Where can I find more information on the combination of the AD5700, AD5421 & ADuCM360 as a smart transmitter circuit?

    The HART enabled Smart Transmitter Demo circuit,  DEMO-AD5700D2Z, developed by ADI, has been compliance tested, verified and registered as an approved HART solution by the HART Communication Foundation. The registration certificate is available from the…

  • AD5421 Chip select and MISO

    Hi

    I'm using AD5421 in my design.

    SPI that I'm using for AD5421 is shared with other device(ADC, another DAC) as well. 

    Whenever I'm using AD5421 I'm ensuring that I have disabled other device using CS to avoid bus contention in MISO.

  • RE: AD5421 Datacode and output current issue

    only change AD5421,different Datacode, same PCBA 

  • AD5421输出电压

        你好,我使用芯片为AD5421BREZ,接入24V电源后,并没有报警电流输出,测得REGIN和LOOP-之间电压为12V,DVDD输出只有1.5V左右,REGOUT配置应该输出5V但只有0.8V左右,REFOUT2输出0.5V左右,REFOUT1没有输出。下面是电路图,请帮忙看一下,谢谢。

  • AD5421 grades

    Hi

    In (AD5421) TUE = Gain + Offset + output drift over temperature + INL

    We can remove gain and offset error as per datasheet.

    So after doing this TUE = output drift over temperature (5ppm FSR /°C ) +INL (0.024% FSR) for A grade (AD5421ACPZ)) and…

  • About AD5421 Iloop under condition

    hello

    My customer is using AD5421, loop power is 24V, now they set the current to 10.2mA,they gradually increased the load RL until the current is drop to 10mA, but the Iloop under bit of the fault register is still at default value , could you pls give…

  • AD5421 Loop supply disconnection impact on registers

    Hi Team

    I'm using AD5421 in my design. In working condition of DAC (When both loop supply and MCU power is available). I'm able to see proper control register value and fault register value is zero.

    When Loop supply is disconnected and MCU power…

  • AD5420 and AD5421 DAC update rate

    Hi

    I'm using AD5421 and AD5420 in my design.

    I have found one observation with respect to both DAC code update rate. I have attached a video file below.

    Click here to play this video

    Here I was setting 4mA, 8mA, 12mA continuously through code. But change between these values…

  • Initializing the AD5421

    Hello, I am working with the AD5421 Eval Board, and I was wondering about how to make sure the AD5421_Init() function provided in the drivers for the device is working properly. More specifically, I want to ensure that the AD5421_SetRegisterValue() function…

  • AD5421 in 3-wire circuit

    I have an existing circuit using the AD5421 as a 2-wire loop-powered transmitter.  It has a CPU, LCD display, sensor ADC, and an AD5700 for Hart transmission.  Works great.

    My customer wants to add additional circuitry that would only be used if the device…