FAQ
Q.
Can the either REG_OUT or DVDD outputs of the AD5421 be used to drive the IODVDD supply pin?
----------------------------------------------------------------
A.
The AD5421 is a loop powered 4 to 20mA Iout DAC. It accepts a loop voltage up to 60V (typically…
Dear Sir, we made the circuit attached using the AD5421.
The loop power is 24V and I use for testing a 120ohm resistor.
Setting of the device is done for 4 to 20mA.
SPI is decoupled using the ADUM 3151 with a clock of 78KHz.
Everything is working, the…
I did the hardware settings based on "POWER SUPPLIES" and "LINK OPTIONS" instructions in UG-250.
I installed the evaluation software.
What are steps to output the current from LOOP- in evaluation software GUI?
The HART enabled Smart Transmitter Demo circuit, DEMO-AD5700D2Z, developed by ADI, has been compliance tested, verified and registered as an approved HART solution by the HART Communication Foundation. The registration certificate is available from the…
应用于HART仪表,使用了AD5421+AD5700套片来实现HART通信,我们自己绘制并焊接了一些开发板,开发板上除了HART套片外还有一个MSP432单片机以及一些放大器。
在实际使用中发现当设定输出4mA时,部分开发板输出为4.6mA、部分开发板一开始输出为4mA随后逐渐变化为4.6mA、部分开发板可以输出4mA。
AD5421使用了4-20mA工作模式,尝试调整了失调寄存器等参数对其没有影响。
开发板上因功耗问题,AD5421输出12V电压,使用了一个LTC3388 DCDC转换器为全板提供3…
Hi
I'm using AD5421 in my design.
SPI that I'm using for AD5421 is shared with other device(ADC, another DAC) as well.
Whenever I'm using AD5421 I'm ensuring that I have disabled other device using CS to avoid bus contention in MISO.
…only change AD5421,different Datacode, same PCBA