• EV-AD5415/49SDZ 輸出電壓調整35V

    EV-AD5415/49SDZ 關於這板子是否可以變更為輸出電壓為35V

    可有建議的OP,我自己挑了一個ADA4610-2ARZ 不知道可以不可行


    另外在AD5415 若搭配ADA4610有甚麼地方要注意的 ?

  • RE: EV-AD5415 EVB was not able to output 35V, any suggestion

    Hi Kevin,

    The addition of gain will have an impact on the noise of the circuit. To minimize the gain noise, a low noise op-amp should be connected to the AD5415 output.

    Please, find the documentation below as reference:

    http://www.analog.com/static…

  • Daisy chain issue with AD5415

    If you are using or plan to use the AD5415 12-bit DAC chip in a daisy-chain configuration, you need to read page 20 of the marked up data sheet attached.  If you are using the SDO output of even a single AD5415, then you also need to see the erratum marked…

  • I have created a new project for the Renesas YRDKRL78G13 board using the "Applilet3 for RL78/G13" tool for AD5415. The problem is that I want to use the board’s screen to display some variables, but nothing appears on it.

    I have created a new project for the Renesas YRDKRL78G13 board using the "Applilet3 for RL78/G13" tool for AD5415. The problem is that I want to use the board’s screen to display some variables, but nothing appears on it.

  • AD5439: crosstalk problem

    We use AD5439 in a signal generator. We found crosstalk between the two
    channels when using the part. However, there is no crosstalk spec in the
    datasheet .Would you please give some suggestion to this problem.

     

    A table of crosstalk measurements…

  • AD5449: Output noise spectral density

    My customer considers to replace AD7568 with AD5449. In their application the
    noise performance between 1Hz and 100Hz is very critical.

    The “Output Noise Spectral Density” they can cope with should be
    <20nV/sqrt(Hz)  @ 10Hz –100Hz…

  • RE: What hardware tools do I need to evaluate my ADI part?

    It depends on the ADI device.

    For those with SDP based product evaulation boards, to evaluate the ADI part using the Analog Devices System Demonstration Platform (SDP) the following hardware components are required:

    • a controller board, like the EVAL…
  • 8/9月热门技术解答帖汇总

    求助AD2S1210芯片信号输入范围问题

    http://ezchina.analog.com/message/18951#18951

    ADV7282-M镜像问题

    http://ezchina.analog.com/message/18953#18953

    电源芯片选型求助

    http://ezchina.analog.com/message/19107#19107

    ADE7878的原理图这样设计有问题没?

    http://ezchina.analog.com/message/19101#…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…