• AD5413 FAQ

    Question 1

    If the AD5413 is configured in current output mode and is driving current into a load, what happens if the loop is open?

    Answer 1

    The current output buffer will run out of head room and flag an Iout Open Circuit Error (IOUT_OC_ERR) in the Analog…

  • AD5413 - capacitive load

    What capacitive load can the AD5413 drive in current output mode?

  • AD5413 - Open loop

    If the AD5413 is configured in current output mode and is driving current into a load, what happens if the loop is open?

  • AD5413 - series resistance

    Do I need to add some series resistance to each voltage sense input to provide some extra protection to the AD5413?

  • AD5413 - output ranges

    Can the device output bipolar ranges from a single supply? Is it possible to supply the DAC in a way that all output ranges are covered? What is the minimum number of supplies necessary?

  • AD5413 - minimum supply

    What is the minimum supply that will satisfy a use case of driving 20mA into max 1K load?

  • AD5413 - internal vs external reference

    The AD5413 integrates an internal reference. How can I configure the part to work with it? Does the part require extra circuitry? If I decide to use an external reference, do I need to reset/reconfigure the part?

  • Does the AD5413 support daisy chaining?

    Does the AD5413 support daisy chaining?