Okay I'm currently working with the AD5391 trying to communicate with it via I2C. I'm very much a newbie so I suspect theres something silly I've missed on the datasheet but I've been trying for a day to find it to no avail so I figured I'd ask…
Okay I'm currently working with the AD5391 trying to communicate with it via I2C. I'm very much a newbie so I suspect theres something silly I've missed on the datasheet but I've been trying for a day to find it to no avail so I figured I'd ask…
I can't believe I have to ask this here, but I can't seem to make sense of the datasheet.
On page 8 in the spec table, it says 0/AVDD (which is what I want)
On page 23 it says VOUT=(2)(VREF)(x2/2^n) which gives 2.5V at x2=4095 because VREF is…
Hello,
I have several question about AD5391 Power-on reset and power up sequence.
1) Power-on reset is powered by DVDD?
2) What DVDD voltage make start Power-on reset procedure?
3) For avoiding un-expected analog ouput, should power up AVDD after…
Hello
What are the maximum values of the output frequency and the sampling frequency? Where is written in datasheet about it?
Hello,
Our part numbers are AD5391-3 and AD5383-3. Though we are using AD5391-5 and AD538-5, here, i only want to use AD5391-3 as example to ask my questions.
1. What's the mean of "boost off" and "boost on"? How can I know if my chips are in boost on…
Hi leixue,
You can use the AD5535B as the LSB is 50V/65536= 3.05mV. you just want to be able to maximize the resolution as the minimum output range is 50V.
Other solution that you can consider is using the AD5391 with a gain amplifier (G=4) at the outputs…
Hello Jino,
I'm glad to get your reply.
1. Our application is PET, so there are many ADI parts used in our system (AD8264/AD603,AD8065,AD8001/8000,AD5391&AD5383,AD9218&AD8138). The AD8001 and AD8000 are used to implement adder, which will provide…
AD693 |
AD5410 |
AD5412 |
AD5420 |
AD5422 |
AD5735 |
AD5755 |
AD5755-1 |
AD5737 |
AD5757 |
AD5421 |
AD421 |
AD5758 |
AD7569 |
AD7669 |
AD7868 |
AD7869 |
AD5593R |
AD5592R |
AD5940 |
AD5941 |
AD7293 |
AD7294-2 |
AD7292 |
AD5590 |
AD7294 |
L… |