• AD9914, AD9959 Eval Software Dev API

    I'd like to be able to interface with the AD9914 amd AD9959 evaluation boards via USB using my own software (written either in C++ or python). This is similar to other posts - see:

    Re: AD5370 Eval - Software Development API - CYPRESS USB (EZUSB…

  • How to get gain(M) from DAC transfer function?

     

     

    I took over someone's codes that set up DAC using AD5373 (32 channels, 14 bit serial input).

     

    In the middle of initializing DAC in C codes, he adjusted gain(M) value in favor of this project, and I don't understand how the M…

  • Using DLL / Labview to program multiple eval-ad5370 boards

    Hi folks,

     

    I have an eval board for the AD5370.

    I have used it and it works very well in various modes.

    My difficulty is summarized in my reply to the 3rd topic in the EngineerZone.

    Re: AD5370, AD5371, AD5372 and AD5373 evaluation board software…

  • RE: AD5370, AD5371, AD5372 and AD5373 evaluation board software commands

    This question has been closed by the EZ team and is assumed answered.
  • FAQ: Selecting A Reference for the AD536x and AD537x DACs

    Q.

    How do I select a reference for the AD536x and AD537x DACs?

    -----------------------------------------------------------------------------------

    A.

    A reference value from +2V to +5V can be used with the AD536x and AD537x. Using the default register…

  • SPI interface to connect to AD5372 in linux via IIO

    The AD5360 IIO Multi-Channel DAC Linux Driver provides a simple way of interacting with AD5360-AD5373 devices vial linux IIO

    http://wiki.analog.com/resources/tools-software/linux-drivers/iio-dac/ad5360

    The question is: what SPI interface hardware (preferably…

  • SPI commands for AD7799 evaluation board

    Hello 

    I´m using this evaluation board to test your AD7799 device. Until now, evaluation software has been succesfull to perform early test but now i need to intregrate my movement device with AD7799 into a Labview application.

    I have read plenty of information…

  • FAQ: X1A and X1B Registers in the AD536x and AD537x DACs

    Q.

    What is the Difference Between the X1A and X1B Registers in the AD536x and AD537x DACs?

    -----------------------------------------------------------

    A.

    Both registers act exactly the same. By default the X1A register is selected. The X1B can…

  • FAQ: Selecting An Output Range for the AD536x and AD537x DACs

    Q.

    How do I select an output range for the AD536x and AD537x DACs?

    ----------------------------------------------------------------

    A.

    The output span of the AD536x and AD537x is principally determined by the reference voltage on the VREFx pins…

  • FAQ: Using the Offset Register in AD536x and AD537x DACs

    Q.

    How do I use the offset register in AD536x and AD537x DACs?

    ------------------------------------------------------------------------------

    A.

    The Offset register sets the offset voltage of a 14-bit DAC. The DAC can be used to move the output…