• AD5370 vs AD5371 Power Up Default Value

    There appears to be a cut and paste error in the AD5370 (16 bit) vs AD5371 (14 bit) datasheets. On page 18 on both datasheets, top of the right hand column it mentions that the default code for X1A and X1B is 5461 for both the 14 bit (AD5371) and the…

  • AD9914, AD9959 Eval Software Dev API

    I'd like to be able to interface with the AD9914 amd AD9959 evaluation boards via USB using my own software (written either in C++ or python). This is similar to other posts - see:

    Re: AD5370 Eval - Software Development API - CYPRESS USB (EZUSB…

  • FAQ: Selecting An Output Range for the AD536x and AD537x DACs

    Q.

    How do I select an output range for the AD536x and AD537x DACs?

    ----------------------------------------------------------------

    A.

    The output span of the AD536x and AD537x is principally determined by the reference voltage on the VREFx pins…

  • AD5383 having difficulty getting an output using SPI

    HI,

    I bought EVAL-AD5383 (obsolete) and I am trying to use SPI to communicate to the DAC.

    A little history on my experience using Analog Devices DAC:

    I have previously evaluated AD5371 using an eval board and then prototyped a design using microcontroller…

  • Using DLL / Labview to program multiple eval-ad5370 boards

    Hi folks,

     

    I have an eval board for the AD5370.

    I have used it and it works very well in various modes.

    My difficulty is summarized in my reply to the 3rd topic in the EngineerZone.

    Re: AD5370, AD5371, AD5372 and AD5373 evaluation board software…

  • RE: AD5370, AD5371, AD5372 and AD5373 evaluation board software commands

    This question has been closed by the EZ team and is assumed answered.
  • FAQ: Selecting A Reference for the AD536x and AD537x DACs

    Q.

    How do I select a reference for the AD536x and AD537x DACs?

    -----------------------------------------------------------------------------------

    A.

    A reference value from +2V to +5V can be used with the AD536x and AD537x. Using the default register…

  • SPI commands for AD7799 evaluation board

    Hello 

    I´m using this evaluation board to test your AD7799 device. Until now, evaluation software has been succesfull to perform early test but now i need to intregrate my movement device with AD7799 into a Labview application.

    I have read plenty of information…

  • FAQ: X1A and X1B Registers in the AD536x and AD537x DACs

    Q.

    What is the Difference Between the X1A and X1B Registers in the AD536x and AD537x DACs?

    -----------------------------------------------------------

    A.

    Both registers act exactly the same. By default the X1A register is selected. The X1B can…

  • FAQ: Using the Offset Register in AD536x and AD537x DACs

    Q.

    How do I use the offset register in AD536x and AD537x DACs?

    ------------------------------------------------------------------------------

    A.

    The Offset register sets the offset voltage of a 14-bit DAC. The DAC can be used to move the output…