• RE: AD537 timing capacitor failure

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD 537JH V to F converter

    Please read the AD537 datasheet carefully.  The  input voltage (of the AD537, i.e. the output voltage of the In-Amp) must be converted to the proper drive current at the input pin by selecting an appropriate scaling resistor.

  • RE: where do i can find AD537JH (V to F Coverter) in LTspice XVII simulator?

    There is no SPICE model for the AD537 - my apologies that I couldn't be more helpful.

    -Anne

  • RE: 150 khz Tape Bias oscillator based on AD537JH

    Hi,

       The AD537 is a voltage or current to frequency converter. In order to produce a stable frequency you need to have a stable and consistent current to drive the AD537. The frequency will change whenever there is a change in voltage or frequency. That…

  • 2009-03-19 03:43:26     adding a module to uClinux kernel

    2009-03-19 03:43:26     adding a module to uClinux kernel

    Yuval Yosef (ISRAEL)

    Message: 71234   

    hi all,

    I am using AD537 blackfin stamp-board/

    I want to add another module to uClinux kernel. I have the device code (it is a Cyrus Logic sound card)

  • RE: 150 khz Tape Bias oscillator based on AD537JH

    Hello,

    It appears that the AD537 would do the job for you. However, I recommend that you double check with the friendly team over at the Precision ADCs board -- this is one of our more general-purpose (read: not audio-specific) parts, so you might get…

  • RE: F-V Converter without AD650

    Hi,

    We have other parts that can be used a F to V converters - the ADVFC32, AD537 or AD652. However, the parts are in cerdip or DIP. The smallest package is the PLCC in which the AD650 is available.


    Thanks and Best Regards,

    Chris

  • RE: LabView Driver for AD5370 Eval Board?

    Thank you for the suggestions and code, after a lot of frustration and wasted time I finally got  LabView to work with the Eval card, just not quite how you suggested.  For others who might try to do the same thing in the future, here is a summary of what…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • AD534KH or AD534KH/+ ?

    Hi,

     

    does anybody know what the /+ (or +) means at the end of the PN of the old AD534xx ?

    The datasheet mentions 2 "/+" versions (JH/+, KH/+) but does not give any explanation of its meaning ?

     

    any idea?

     

    Thanks.

    FP