• RE: AD5360 Eval Board Communication

    Dear colleagues,

    I am not sure if the question from Joshua has been addressed, but I am personally still confused by the answer. I'm very new here, so maybe I am missing something, but I couldn't find the source code for the hex-file in the reply by ADIApproved…

  • Whether the output of LTC2668 and AD5360 is synchronous and in-phase

    Are there any way to set all Vout pins of the LTC2668 and AD5360 to output synchronous and in-phase? If there is a way to achieve it, how should it be implemented?

  • AD5360开发板win10驱动程序

    AD5360开发板有win10驱动程序,官网只有win7的,或者怎么安装那个对应的软件有正确的驱动程序呢?

  • LTC2668和AD5360输出是否为同时同相位?

    LTC2668和AD5360的16个输出通端口中输出的数据是一次输出一个Vout端口中,还是可以一次性将所有Vout端口设置为同时同相位输出,如果可以同时输出应该如何设置

  • Interfacing DAC AD5360 with Arduino Mega

    Hello I am trying to interface AD5360 and Arduino Mega using SPI ,

    I am sending commands given as per the datasheet however not getting any analog output. RESET and BUSY pins are working as expected but when I try to toggle the GPIO of the DAC it always…

  • connect 2 or more ad5360 devices together

    Hello everybody,
    as the title suggests I am trying to connect 2 or more ad5360 devices together with LV.

    Using the "search for board" function this gives me 2 "path" values ​​but when I try to do the init on the second it does not return a handle.…

  • connect 2 or more ad5360 devices together

    Hello everybody,
    as the title suggests I am trying to connect 2 or more ad5360 devices together with LV.

    Using the "search for board" function this gives me 2 "path" values ​​but when I try to do the init on the second it does not return a handle.…

  • Connect 2 or more ad5360 devices together

    Hello everybody,
    as the title suggests I am trying to connect 2 or more ad5360 devices together with LV.

    Using the "search for board" function this gives me 2 "path" values ​​but when I try to do the init on the second it does not return a handle.…

  • AD5360 的所有输出通道可以将数据同时输出吗?同时输出的时候会有相位差吗

    ad5360接收来自fpga的数据后,经过数模转换需要同时将所有数据同时输出,输出时不能有相位差,可以实现吗

  • Compiling a linux kernel for AD5360

    Hi, I'm having some issues trying to compile a raspberry pi kernel to use for my EVAL-AD5370 board.

    I've followed the following sites:

    https://wiki.analog.com/resources/tools-software/linux-build/generic/raspberrypi

    https://linux.ime.usp.br/~marcelosc…