• AD5338: Difference in offset between channel 1 and channel 2 of the AD5338

    Hello, by testing more or less 10  AD5338s I find an offset from 3mV to 17mV
    only for 2nd channel VoutB (PIN3)
    while VoutA (PIN2) has no offset. I tested the pin with no load. The amount of
    offset is in the tolerance (from datasheet) but I don…

  • RE: Connecting Vref on AD5338R

    Hi,

    Apologies for the delay.

    The AD5338R has a common reference pin. When using the internal reference, this is the reference output pin. When using an external reference, this is the reference input pin. The default for this pin is as a reference output…

  • Is ADP2291 working as expected in the datasheet or its examples are fail?

    Hello Everyone,

    Im working on a battery charger circuit. I set completely the figure-22 and the figure-23 in the datasheet. So more than hundred try and later than weeks. The circuits are not working as expected. This part is important "The circuits are…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • ADI芯片辨识、型号查找

    看看截图: