在进行了ADL5330测试时,发现在任何频率下总是达不到手册中给出的60dB动态,有了解的帮忙指导一下!谢谢大家
I am using this chip for the very first time. I am confused with cs, wr, ldac and clr pins. plz let me know what is the configuration
Hi Dina,
If you only use one device, you can directly connect the /CS pin to your microcontroller.
Can you check AD5330, that's a newer 8-bit, parallel interface DAC.
Cheers,
Ivan
Hi, Joel;
Thank you for the reply. Now I know AD5330 is suitable for Transmitter.
And since AD8357 is a 200 ohm system, should I insert a 4:1 tranformer at its output port, or as the demo circuit we insert 174/57.6 ohm resistors? which way is best?
Hi Thomas,
Yes there is a simple solution. Actually simplicity is in the eye of the beholder, so let's just say there is an all-analog solution and it uses the AD8302, which is a gain and phase detector. Still, it is easier than digital predistortion…