• EVAL-AD5324 and EVAL-SDP-CB1Z LabView/LabWindows Application

    Hello,

    I'm trying to develop an arbitrary waveform generator using an EVAL-AD5324 and an EVAL-SDP-CB1Z using either LabView or LabWindows.  It'll be pretty simple waveforms, mostly a combination of DC and square waves at 60Hz of various amplitudes…

  • Is AD5624 a possible replacement for AD5324?

    We are looking at alternates for the AD5324 (mainly for cost reduction), and it seems that the AD5624 is a good candidate. Would the AD5624 be considered a very close replacement for the AD5324? The current DAC is used in a low speed correction loop with…

  • AD5324

    I using AD5324 for Voltage out control, but I face the problem when the MCU’s SPI interface between the AD5324 & PLL (from RF board) together, the AD5324 will “hang” which suspect the noise from RF cause the AD5324 “hang”. During this situation, MCU write…

  • DAC输出跳变问题!

    大家好!

            我想请教一个问题,我最近用AD5324用来产生模拟电压。当AD5324输出电压以步长0.05V/0.1秒,从0.5V变到0.8V的过程中,输出电压会出现超过1V的跳变,然后又恢复过来。最终输出停在0.8V,请问为什么会出现这样的跳变。

            单独设定输出电压都是对的。我检查了,AD5324四个输出通道只要电压从小到大变化时,过程中都会出现很大的跳变,然后又恢复正常。

           

    请大家赐教!谢谢!

  • Vdd2(Secondary side) question for ADuM1300 CN0064

    Dear Sir /Madam,

    Question-1

    Can we use your ADR02 as VDD2 of ADuM1300 due CN0064 reference circuit?

    Our customer choiced your ADuM1300 and AD5324,so he is studying now about VDD2.

    Your CN0064 show to use ADR02 Vref as power device.

    Bur your DAC on…

  • RE: AD5328 ibis model?

    Hi,

    Unfortunately, we dont have specific model for the AD5328... just in case I attached the AD5324...

  • DAC and SPI with DMA

    I want to transmit data to AD5324 DAC using SPI with DMA but as with most non-audio DACs it requires a pin toggle to latch data in the DAC buffers after each TX. There is a Chip select associated with each SPI port on the STM32F407 micro that I'm using…

  • Is ADP2291 working as expected in the datasheet or its examples are fail?

    Hello Everyone,

    Im working on a battery charger circuit. I set completely the figure-22 and the figure-23 in the datasheet. So more than hundred try and later than weeks. The circuits are not working as expected. This part is important "The circuits are…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • ADI芯片辨识、型号查找

    看看截图: