• AD5322 offset error

    Helo.

    I use DACs AD5322. In channel A offset error voltage 21mV, if i write code 0x000 to DAC register. In channel B offset voltage 4.5mV. And it offset save for all power band, until Vref. In this case voltage output = Vref+offset error voltage.

    This…

  • [AD5322] Deasserting SYNCb before 16th clock edge

    Hi,

    What should be happen in input shift register when SYNCb is deasserted before 16th falling edge of SCLK?

    My expectation is that the content of the input shift register should be cleared and the content of the input register should not be changed…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • AD5312 Lock up

    We are using an AD5312 that works flawlessly.  It outputs the analog values we are looking for and all of the control signals look good.   The problem we are experiencing is that occasionally during electrical noise it locks up and begin to Output 3 volts…

  • AD5312 and LDAC

    Please confirm that if the LDAC pin is held low, then the data is clocked straight through from the input register to the DAC register. Please clarify at what instant does the DAC change its output value (after the 16th bit is clocked in? after the SYNC…

  • AD5302 and LDAC control

    I was wondering if something could be done with the LDAC pin because on all the application shown at the end of the datasheet, LDAC is often not represented. I want to keep LDAC low but Im not sure if this can be done. Could you please confirm?