• AD5321 power down

    Hello,

    Will pulling the PD pin low also reset the DAC device I2C bus logic? I'm not looking to reduce the power consumption, but to reset the device.

    I read that many I2C devices can latch, blocking the whole bus from operation, and it is recommended…

  • About AD5321 I2C Timing

    Hi,

    My customers say they want to use AD5321.
    I got a question there.

    #1 Does that mean that SDA must be switched within 0.9 μs of the max value of data hold time at t 6?

    #2 What is the problem when I exceed the max value of data hold time of t6 in…

  • AD5321_I2C level translator

    We use 5V to power the AD5321, and use 3.3V FPGA to control the serial port of
    AD5321. We connected pull-up resistor to 3.3V on the SDA and SCL Pins. We can
    control the AD5321 correctly by I2C Port, but I checked the datasheet, the
    input high…

  • RE: HMC8205BF10 Required Power Supply

    Hi Saravana,

    The 8205 is a CW part.  Do you need it pulsed or need gate control?  If so, unfortunately we do not have any Automatic Bias Control parts at 50V.

    I cannot provide a full schematic yet but I do have a block diagram with a way to control the…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • ADI芯片辨识、型号查找

    看看截图: