• AD5320

    Hello!

    On my microcircuits AD is absent marking fist output? How detected first output when I will solder circuits? 

  • AD5320 spice

    Do you have spice model for AD5320?

    Thank you

  • AD5320 DAC has no output

    Hi ADIexpert

    My customer is using AD5320 as a DAC to output different voltage for its motor control application

    however, no output was found (always 0V at the Vout) for different data 

    please see the SPI diagram from MCU and schematic below

    Ch1: x1…

  • RE: AD9833 and AD9834 specification on CPOL and CPHA

    Hi Miguel,

    Thanks for the quick response. This typos raised a concern. Could you confirm if the AD5300, AD5310 and AD5320 datasheets are correct? They mention that CPOL = 0 and CPHA = 1, but they don't mention if SCLK is active high or active low, so…

  • 几款AD及DA芯片

           AD公司生产的各种模数转换器(ADC)和数模转换器(DAC)(统称数据转换器)一直保持市场领导地位,介绍几种AD及DA芯片,结构包括了高速、高精度数据转换器和目前流行的微转换器系统(MicroConvertersTM )。  

           1)带信号调理、1mW功耗、双通道16位AD转换器:AD7705   AD7705是AD公司出品的适用于低频测量仪器的AD转换器。它能将从传感器接收到的很弱的输入信号直接  转换成串行数字信号输出,而无需外部仪表放大器。采用Σ-Δ的ADC,实现16位无误码的良好性能,片内可…

  • RE: ADI 12位的adc 和DAC转换  有没有?

    对于ADC 12bit 8pin脚的产品,您可以考虑AD7893、AD7895(但是这两款都是外部参考);AD7896是内部参考。

    对于DAC产品,您可以考虑:AD420;AD5320和DAC8512。

  • RE: 发帖就送话费啦(限前一百名哦),还有大奖等您拿(获奖名单已公布)

    AD公司生产的各种模数转换器(ADC)和数模转换器(DAC)(统称数据转换器)一直保持市场领导地位,包括  高速、高精度数据转换器和目前流行的微转换器系统(MicroConvertersTM )。   1)带信号调理、1mW功耗、双通道16位AD转换器:AD7705   AD7705是AD公司出品的适用于低频测量仪器的AD转换器。它能将从传感器接收到的很弱的输入信号直接  转换成串行数字信号输出,而无需外部仪表放大器。采用Σ-Δ的ADC,实现16位无误码的良好性能,片内可 编程放大器可设置输入信号增益。通过片内控制寄存器调整内部数字滤波器的关闭时间和更新速率…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • ADI芯片辨识、型号查找

    看看截图: