• AD5318: locked status due to power on

    When a slow power up ramp is used, I have problems getting the device to power
    up correctly. The only solution is to turn off the power, then turn on again.
    The design follows the evaluation board, 0.1uF and 10uF CAP are added to the
    Vdd.
    The…

  • DAC selection: Is there a better recommended choice for new design than AD7805?

    For a new design we want use DAC AD7805. Is it advised to use it for a new
    design? Our requirements :
    - min 3 DAC outputs.
    - min resolution 10 bit.
    - input format : parallel.
    - power supply +5V.
    - signal input : 0V min > 5V max 0Hz min >…

  • AD8567: Connect the device paddle

    We're using your AD8567 (2 pcs) as buffers for our internal 8-channel DAC
    (AD5318). The used chip housing (LFCSP16) has got an exposed pad on the bottom.
    Do I have to connect this pad to ground (to improve the electrical
    characteristics…
  • 【ADI参考代码集!AD7192 AD7150 AD9912...】有更新!——2

    模数转换器 (ADC):

    AD6657 | AD7150AD7190 | AD7191 | AD7450 | AD7606 | AD7705 | AD7709 | AD7718

    | AD7719 | AD7730 | AD7734 | AD7746 | AD7780

    AD7783 | AD7791 | AD7792 | AD7794 | AD7862 | AD9272 | AD7192 |

    AD7264

    NEW! |

    AD7265

    NEW!

       

    数模转换器…

  • 【ADI参考代码集!AD7192 AD7150 AD9912...】有更新!——1

    模数转换器 (ADC):

    AD6657 | AD7150AD7190 | AD7191 | AD7450 | AD7606 | AD7705 | AD7709 | AD7718

    | AD7719 | AD7730 | AD7734 | AD7746 | AD7780

    AD7783 | AD7791 | AD7792 | AD7794 | AD7862 | AD9272 | AD7192 |

    AD7264

    NEW! |

    AD7265

    NEW!

       

    数模转换器…

  • AD5308 Serial Interface?

    Here is my question.

    We want to send the AD5308 a 10-bit value instead of 8-bit for reasons of software compatibility.

    The AD53x8 datasheet isn’t clear on this, it says:

    The AD5318 uses 10 bits and ignores the 2 LSBs. The AD5308 uses 8 bits and ignores…

  • RE: AD5328 ESD

    The ESD rating for the AD5328, AD5318 and AD5308 is class-3 or 4kV. This implies it an extremely robust device.

    ESD failure threshold classification is as follows:

     

    CLASS 3 4,000 VOLTS AND ABOVE

    For further information on ESD visit the Analog Devices…

  • AD5318_8通道数据传输

    从数据手册的图2可知,SYNC信号应在第16个时钟周期后拉高。我的疑虑是,能否一次性传输8个16位数据(8通道数据),并使SYNC保持低电平,直到第8个数据从DIN传输完毕为止?然后拉低LDAC,更新所有数据以同步输出。这样可以吗?还是每传输16位数据就必须切换一次SYNC?

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…