Hi,
Is there internal pull-up or pull-down resister on serial interface pins (SYNCb, SCLK, DIN) for the AD5312?
Regards, Satoshi
Hi,
Is there internal pull-up or pull-down resister on serial interface pins (SYNCb, SCLK, DIN) for the AD5312?
Regards, Satoshi
Hi
Q1. If the reference input of AD5312 become 0V during the buffered mode, what AD5312 happen ?
Q2. The customer hopes the reference voltage performs ON/OFF control of Vout regardless of buffered or unbuffered. Is it possible ?
Regards,
Hiroyuki
We are using an AD5312 that works flawlessly. It outputs the analog values we are looking for and all of the control signals look good. The problem we are experiencing is that occasionally during electrical noise it locks up and begin to Output 3 volts…
Hi,
What should be happen in input shift register when SYNCb is deasserted before 16th falling edge of SCLK?
My expectation is that the content of the input shift register should be cleared and the content of the input register should not be changed…
Hi everyone,
I'm facing a weird problem with a sport on ADSP-21161.
The sport is used to drive a AD5312 DAC: I configure it for data transmit, internally generated clk and fs, late frame sync, active low.
I've always used it in data dependent mode…
I was wondering if something could be done with the LDAC pin because on all the application shown at the end of the datasheet, LDAC is often not represented. I want to keep LDAC low but Im not sure if this can be done. Could you please confirm?
AD693 |
AD5410 |
AD5412 |
AD5420 |
AD5422 |
AD5735 |
AD5755 |
AD5755-1 |
AD5737 |
AD5757 |
AD5421 |
AD421 |
AD5758 |
AD7569 |
AD7669 |
AD7868 |
AD7869 |
AD5593R |
AD5592R |
AD5940 |
AD5941 |
AD7293 |
AD7294-2 |
AD7292 |
AD5590 |
AD7294 |
L… |