• AD5311R Logic output current

    Hi,

    My customers are considering using the AD5311R.

    So I got a question.

    It is about Logic Output (SDA).
    In the test condition, Isink = 200 uA, Isource = 200 uA,

    but if Isink = 2 to 3 mA, Isource = 2 to 3 mA, will the values of VOL Max, min change…

  • AD5311R Output Logic Current(test condition)

    Hi,

    My customers are considering using the AD5311R.

    So I have a question.

    It is about test condition of Logic Output (SDA).
    Where Isink and Source are Sink and Source?

    Is it the transmission line to the load?

    Best Regards,

    Yuya

  • RE: ADI_TWI_BUFFER_ERROR reason?

    Hi jcolao,

       my company is use SC589 in product, not evaluation board. I had modified the eval board example(ReadVoltage_SC589_Cortex) to communicate with ad5311r(a I2C device). The error was happened when write data to it. Read data from it not test current…

  • Can the AD5310R "SHORT WRITE OPERATION"?

    Hi

    My customer is considering AD5310R.


    The AD5310R data sheet says “If SYNC is high after 16 falling clock edges occur, it is interpreted as a valid write and the first 16 bits are loaded to the input shift register.”
    However, SPI Command Operation…

  • RE: 电源芯片选型求助

    如果要实现输出电压可调的话,而且您现在需要输出的电流并不是很大,可以考虑用DAC来实现,如AD5310R,AD5311R,AD5693R等芯片。

  • Question about the input of AD5310R

    Hi
    Is the input data stream for the AD5310R correct at 16 bits long?

    The chapter of "AD5310R SPI SERIAL DATA INTERFACE" of the data sheet is as follows.
    "The SYNC pin must be held low until the complete data-word (16 bits) is loaded from the…
  • nanoDAC+ Family AD531x/AD568x/AD569x/AD567x FAQ

    Q1. What is new?

    A1. The nanoDAC+(TM) family offers improved analog performance in terms of INL and glitch energy specifications.. Some members of the family, those with a part number ending in 'R', for example AD5686R, include a  low drift…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…