• AD5308 Serial Interface

    I have a number of AD5308 devices which do not reliably set their outputs. The timing of the SCLK, SYNC, LDAC, and DIN all appear well within range and the device temperature is nominal (Not warm at all).  When I lightly freeze the device with freeze spray…

  • AD5308 reference input


    Hi All,

    I'd like to know whether or not an REF192 can be used for reference of four AD5308 ICs simultaneously.

    Could you tell me about it?

    Best Regards,

  • AD5308 Serial Interface?

    Here is my question.

    We want to send the AD5308 a 10-bit value instead of 8-bit for reasons of software compatibility.

    The AD53x8 datasheet isn’t clear on this, it says:

    The AD5318 uses 10 bits and ignores the 2 LSBs. The AD5308 uses 8 bits and ignores…

  • AD5308 stability of output amp when driving cap loads

    From the AD5308 data sheet

    OUTPUT AMPLIFIER

    ........The output amplifier is capable of driving a load of 2 kΩ to GND or VDD, in parallel with 500 pF to GND or VDD. ..........

    Is it a valid conclusion that the output amplifier, when configured for…

  • a DAC with 8V output

    Hi,

     

    I am looking for a chip with 8 DACs which can provide 0-8V at the output. Specifically, I am looking for a chip similar to AD5308 but with higher output voltage.

     

    Application: adjust the voltage at the control lines of  8 analog phase sifters…

  • RE: AD5328 ESD

    The ESD rating for the AD5328, AD5318 and AD5308 is class-3 or 4kV. This implies it an extremely robust device.

    ESD failure threshold classification is as follows:

     

    CLASS 3 4,000 VOLTS AND ABOVE

    For further information on ESD visit the Analog Devices…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…