• AD5301: Reference usage

    Part Nr.: AD5301/5311/5321
    I plan to use your DA converters on a board,
    giving the possibility to my fab plant to select
    any of the three refs mentionned above, depending
    on components availability, as I only need 8 bit
    resolution.
    My question…

  • AD5301 Signal Accuracy and Absolute Error

    I am using the AD5301BRM. THe datasheet states the accuracy is 1LSB.

    1. Is such accuracy correct for AD5301BRM?

     

    1. You should indeed get a result of 1 LSB if you are measuring correctly.
    Did you notice "note 4" at the bottom of page 2 of the…

  • Example IIO driver code for the I2C AD5301

    Hello, 

    A customer is trying to use the IIO driver for the AD5301 I2C DAC.  He found this page that shows example driver code for numerous DACs including the AD5301, but the code appears to be focused on the SPI interface instead of I2C. 

    AD5446 IIO DAC Linux…

  • How can I calculate the max. output frequency of AD5301 DAC

    Hi. Im trying to calculate the max output frequency of AD5301 DAC. I checked the AD5301's datasheet to calculate it. However, I could not find the sampling rate of this IC. Maybe I missed something important point on datasheet. Anyone can brief me…

  • RE: i2c read write to AD5301

    This question has been closed by the EZ team and is assumed answered.
  • Photosensitivity of CSP packages

    I noticed that the ADP5301 in a CSP package shuts down immediately when exposed to direct sunlight. This is similar to that discussed here for a different chip:

     https://ez.analog.com/power/w/documents/4803/faq-photosensitive 

    My suggestion is that all…

  • RE: AD5310 vs AD5601

    Hi Yvan,

    The AD5601 is SPI which is more popular than the AD5301 which is I2C. What is your appication?

    Regards,

    Padraic

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • ADI芯片辨识、型号查找

    看看截图: