• AD5300 SPI start up time

    This is a question from my customer.
    How many seconds after the power on will the SPI communication of the AD5300 become possible?

    Best regards
  • RE: AD9833 and AD9834 specification on CPOL and CPHA

    Hi Miguel,

    But can I rely that, in the case of the AD5300 family, CPOL ins indeed 1 and CPHA is indeed 0?

    Kind regards, Samuel Lourenço

  • RE: AD7789 24bit ADC data register read issue (Arduino)

    Thank you all for the quick response! Yes the SPI line is shared with a 8 bit DAC (AD5300), but the DOUT line is only connected to the AD7789 (DAC only has DIN). The 10 bit ADC I was talking about is one that is built into the Arduino, so it doesn't connect…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • Is ADP2291 working as expected in the datasheet or its examples are fail?

    Hello Everyone,

    Im working on a battery charger circuit. I set completely the figure-22 and the figure-23 in the datasheet. So more than hundred try and later than weeks. The circuits are not working as expected. This part is important "The circuits are…

  • ADI芯片辨识、型号查找

    看看截图: