FAQ
Hi there,
I was hoping to get some help installing the evaluation software for the AD5259. During the install process I come across the below error (image included).
I tried to search up possible solutions to the issue and one such post suggested ask…
Hi,
My customer has used old evaluation board of AD5259 which name is AD5259EVAL but currently this board was obsoleted. So customer consider to buy latest one named EVAL-AD5259DBZ (and EVAL-SDP-CB1Z).
The questionis , can we use software of AD5259EVAL…
Please teach me I2C line of AD5259
SCL, SDA pin it will pull up as shown in Figure 46 and 47.
But,the power supply circuit of the MCU and AD5259 has been separate.
It is a circuit configured to pull up the SDA,SCL by using the power of the MCU.
When the…
Hi
AD5259 power up sequence is
GND, Vdd, Vlogic ,digital inputs and then VA,VB,VW.
Power down sequence should reverse this, I think.
Does AD5259 accept Vdd=VA=VB=VW=0V and Vlogic=5V ?
Abso max accepts this, so it should be ok, I think.
Could I make…
Hi
Please let me know about these fundamental questions of AD5259.
Datasheet says
RWA(D)={(256-D)/256}XRAB + 2 X Rw (2)
Total wipe resistance Rwb is 75 ohm typ @ Code 0x00
What is the relation between these specs and Zero scale Error?
2X Rw = Rwb…
Hello
we want to use the AD5259 in a design.
In the doc is no device adress noted.
If i read the doc in the right way, there is a change over the
whole adress by setting ad0 pin. Normally there is a change of only 1bit.
On this device the change…