• AD5243 VOL output logic level

    I am searching for the Vol (output low voltage level) as the I²C pins are also
    open-collector outputs! What's the value for Vol?

     

    Based on the simulations for a worst case conditions, the max Vol is around
    80mV for 4mA sink. (see attached…

  • Negative output voltage in Dig Pot AD5243 or AD5242

    Hi,

    Could you please clarify the following statement that I found in the datasheet of the above mentiuoned devices: "The digital potentiometer easily generates a voltage divider at wiper to B and wiper to A, proportional to the input voltage at A to…

  • AD5243 INL confusion.

    I am little confused about the INL spec. It is in terms of LSB, but they are in decimals. How is this derived? Is it saying that (for example, on figure 13) if I put a input code of 64, that the whole bit can be truncated by a little over 10% of its whole…

  • About AD5423 Evaluation Board

    Hi,
    My customers are considering using the AD5243 and evaluating it on the evaluation board.
    So I got a question.

    When considering the rheostat mode using B1 and W1, is it possible to open the jumper pins of the evaluation board A20 even if it is open?

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • ADI芯片辨识、型号查找

    看看截图: