• Use of AD5228 with capacitive touch sensor

    Hi  I am planning on using the ad5228   With a capacity touch sensor To drive A555 chip. I realized the AD5228 has Built-in D bouncing, my question is , will the up down pins on the ad5228  will they accept the output from the capacity touch sensor.  Capacitive…

  • possible to use AD5228 as stereo volume control?

    Hi,

     

    I am wondering if it is possible to use two AD5228 to perform as volume control for stereo signal? I am planning to use one up and one down button to achieve it.

     

    I am thinking to connect PU of two digipot together (same to PD), so that i can…

  • RE: AD5162, "A" terminal for second channel

    Hi Usaghi,

    On page 16 of the AD5228 datasheet (Rev A.) there is a brief article on using the AD5228 in an audio amplifier with volume control.

    There is also a detailed circuit note that's worth looking at also: http://www.analog.com/static/imported…

  • RE: Two AD5116 + One SSM2306

    Hi Musach,

    So do you mean to replace the SSM2306 with other op-amp?

    I still prefer to use SSM2306 as it proves to be a good class-D audio amp for me. Any other way to use the AD5116 with SSM2306?

    By the way, to use one set of buttons to control two…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…