• AD5206: Timing

    Does the DP work with CS at clock falling edge or rising edge?
    And what about the SI clock falling or rising edge?
    At which frequency it’s recommended to work with the DP?

     

    Data is clocked in from SDI on the rising edge of CLK and clocked…

  • ad5206 problem

    Hello,

    I'm using the exact same digipot (AD5206) . When I measure the impedance across A and B for any channel on the digipot, I get a very high reading of a few Mega ohms, even though my digipot is 10kohm. The datasheet shows that there is no SHDN…

  • AD5206 DigiPot Broken?

    Hi all,

    I'm having trouble with my AD5206 10kohm digipots in the discontinued PDIP form. For some reason, all channels are reading excessive impedance (in the mega ohm range) between any combination of A, B, and W. This is with the Vss, Vdd, GND, and…

  • RE: RDAC AD5206: doesn't works like i need it

    This question has been closed by the EZ team and is assumed answered.
  • RE: AD5206 occasional setting error

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD5206 trailing numbers

    Can someone tell me if these are the same AD5206? Are the trailing numbers just a batch/serial number?

    See attached photo.

  • AD5206 wiper position problems

    Hello,

    I am currently designing a PCB so that I can take a single 40kHz input signal and by using two AD5206 100kOhm digital potentiometers, have four output signals which I can phase shift and magnify. The issue I'm running into is this: not all of…

  • On the rated values of Ia, Ib, Iw of AD5206

    Hi,

    I would like to use AD5206.

    So, I have a question. Please help me.

     

    Question:

    In the data sheet, there are two description of the rated values for Ia, Ib, Iw.

     

    One is defined as "Continuous 10 kΩ End-to-End Resistance ± 11 mA" in the Absolute…

  • AD5206 inconsistent value settings

    I breadboarded a simple circuit to check the functionality of using the AD5206 in rheostat mode to simulate RTDs for a battery management system.  I find that the resistor setting is incorrect around 1/10 of the time when the same instruction is given…