• RE: Controlling a digital potentiometer (AD5142) by Arduino Uno

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD5142 maximum current

    Hello

        I'm a starter on using AD5142 and notice the maximum current of Ia Iw Ib is just 6mA, does that mean if I connect W to Vdd and A to GND, then program code to reduce Rwa, the chip will get permanent damaged?(Vdd=5V, single power supply, Vss=GND…

  • RE: Is there a table on which SPI DigiPOT is compatible with which other ones?

    Exactly that is why I have asked.

    The datasheet of the AD5122/AD5142is a bit cryptic with the actual SPI mode (and if I recall correctly, the AD5292 is silent about mode at all).

    It would be just good to hear "yes, the AD5142 fits into a chain of AD5292s…

  • AD5141_datasheet

    Please let me know  about  "Figure 19. Rheostat Mode Temperature Coefficient ((ΔRWB/RWB)/ΔT × 106 ) vs. Code " described on p.15 of the datasheet.

    If you look at the datasheet of AD5121, the horizontal axis of the above items…

  • I2C Code Example - AD5142A

    I need to get a Digital Potentiometer (AD5142A) up and running quickly using I2C.  Can anyone point me to an I2C code example initializing and commands for the AD5142?  ad5142a

    Thanks!

  • 最新中文资料更新20130925

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…