FAQ
I want to use 100K Digital Potentiometer
Looking at the data sheet for AD5121 / AD5141, 10k ohms / 100k ohms
AD5121: 10K ohm
AD5141: 100K ohm
Is it okay to think this way?
Hi all
I wanted to ask AD5141 ESD test Method, and what is the ESD withstand voltage of AD5141?.
Could you tell me the ESD test method of AD5141 and ESD AD5141.
Regards
Hi,
My customer is considering using the AD5141 evaluation board.
However, when the evaluation GUI is launched and the evaluation board is connected, the evaluation GUI shuts down.
SDP-S is also connected.
I checked the device manager, I can confirm it as…
Hi,
Can I use the AD5141 to replace both resistors in the feed back loop of a switching power supply? Should I use potentiometer mode or linear gain setting mode?
Thank you.
Dear all,
We are using a FPGA platform with an integrated ARM working under Linux.
For our new Hardware we want to use the AD5141 with the I²C interface.
Is there any Linux driver available for the AD5141 digital potentiometer?
Or is there any guideline…