• AD5115 Digipot

    I have one technical question regarding the digipot AD5115 we are currently
    using:
    1. Wwhat is the default value in the EEPROM of the device after the
    manufacturing? MIN, MAX/2, MAX or undefined value?
    2. Can we use this value in production…
  • AD5111, AD5113, AD5115: Shutdown mode

    AD5111, AD5113, AD511: How can I put the chip in Shuntdown mode?

     

    The command for SHUTDOWN MODE is sent by a low-to-high transition on the U/D
    pin, when CLK is high and CS is enabled. The command is executed on the CLK
    negative edge…
  • AD5115/3/1 pull-up or pull-down requirements

    What are the requirements for pulling up or down the #CLK, U/#D, and #CS pins?  Can I leave them floating?

  • AD5111, shutdown mode

    Hi,

     

    I had a question on AD5111 shutdown mode which is described in datasheet page 18 (Rev.B) as follows.

     

    The AD5111/AD5113/AD5115 return the wiper to prior shutdown position if any other operation is performed.

     

    Q-1) What is the meaning of "prior…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…