• AD5060 Ground Voltages

    Could you tell me which is the absolute maxim rating voltage between AGND
    and DACGND?

     

    0.3V is the normal maximum rating between grounds.
     

  • AD5060 as replacement for AD5040

         Can the AD5060 be used as a drop-in replacement for the AD5040 -- e.g. not just pin compatible but would work in an existing application with its existing SPI sequences.

         Thanks, Bob

  • AD5060

    AD5060单极性工作模式的输出电压计算公式是什么?

  • Where should I connect DACGND of AD5060?

    AD5060 has two grounding pins: AGND and DACGND.

    DACGND is described as "DAC core ground input".

    I'm pretty accustomed to A/D circuits having different ground terminals for digital and analog parts, and if DACGND was labeled as "Digital ground…

  • RE: What is the difference: AD5060, AD5061, AD5062 and AD5063?

    This question has been closed by the EZ team and is assumed answered.
  • RE: AD5040, AD5060, AD5061, AD5062 and AD5063 evaluation board software commands

    This question has been closed by the EZ team and is assumed answered.
  • RE: AD5060 Eval LabVIEW driver not working.

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • What are the AD5060 command definitions?

    Hello All,

    Can someone tell me where to find the complete command definition information for the AD5060?

    I do not see a table like that in the AD5064 datasheet.

    Thanks In Advance,

    John W.

  • 关于AD5060的输出电流

    准备使用的AD5060作为精密的DAC,但是查看数据手册没有发现它的输出电流特性。