There is an error on the Rev D ( and prior ) datasheet, where it is mentioned that a PDL bar (Power Down Lockout) pin can be used.
These parts do not have a PDL pin.
That pin and funcitonality DOES exist on their Dual channel syblings - the AD5025,…
nanoDACs are a portfolio of products which combine small package, low power and low cost digital to analog conversion.
nanoDACs are monotonic DACs which can be powered off a single 3V or 5V supply and are available in the industries smallest packages…
It must be stressed that depending on the application performance requirements, all nanoDACs can be used in both open and closed loop systems.
In an open loop application the DAC drives the load (a valve or an actuator, for example) directly while in…