• Problem Reading Temperature on AD4695

    I am trying to read the temperature sensor on the AD4695 in Single-Cycle Command Mode. I have enabled the status bits and can verify that all the other channels read ok (I am getting the correct index of the channel back). When I go to read the temperature…

  • AD4695 's SDO pin remain High in conservation mode.

    Hi,

    I have implemented and tested all the register configurations. I have read what I have written to the specific register. I check it on the oscilloscope

    also. I think there is no problem with my hardware. After register configuration is done. I give…

  • AD4695 no activity on SDO, always high-Z

    Hi, 

    We are currently developing a board using 3 AD4695BCPZ ADCs connected to the same SPI bus. We are experiencing an issue where no data is appearing on any of the SDO pins of the ADCs - all 3 SDO pins are connected onto a common MISO line but it remains…

  • Linux-IIO support device selection for GSoC'21

    Hi All,

    [I'm not sure whether this is a right place to ask this question or not]

    This is Mugil an Undergrad student from India. I wish to participate in GSoC'21 TLF's IIO project. In that, we need to create a driver for one of the ADI's device…

  • Precision Low Power Signal Chains: A Unique AC Coupled Solution with Configurability

    In last month's blog post we discussed the tradeoffs between AC and DC coupled signal chains when measuring small signals in the presence of much larger DC offsets and low frequency interferers.  We also showed that the location of the high-pass filter…

  • ADN4695E bus termination in a point-to-point topology

    We're using ADN4695E in a point-to-point topology with a 100Ω termination at line end.

    ADN4695E datasheet says "Supported bus loads: 30 Ω to 55 Ω".

    But we're not sure if it's for a multi-point bus, as AD4695E is suitable…

  • RE: AD7682 SAR ADC Design considerations

    Thanks for your question, as you have highlighted the AD7682 is a 16bit 4 channel 250ksps PulSAR ADC, this ADC is an excellent choice for low power data acquisition, and as you have correctly pointed out the power scales with throughput. The AD7682 can…

  • ADN4695E bus termination in a point-to-point topology

    We're using ADN4695E in a point-to-point topology with a 100Ω termination at line end.

    ADN4695E datasheet says "Supported bus loads: 30 Ω to 55 Ω".

    But we're not sure if it's for a multi-point bus, as AD4695E is suitable for, or if it…