FAQ
Hi
I use the top circuit for drive the AD421. To get the current of 4-20 mA, should an external power supply be used instead of Vloop?
And should be resistor series to an external power supply and the voltage across the resistor be the same as the current of…
I do not use the DAC's functionality, only its 3.3V output to power the MODEM to communicate HART over the loop.
I do not want to have to add circuitry to write the DAC's loop current register.
What is the default loop current?
Will a AD5700 HART…
请问AD421的环路电流建立时间8ms是否指每次给421芯片一个数字量后,421转换为电流信号的稳定时间,还是指代初始化时电流稳定时间。
我现在AD421的前级是一个转速为5000rpm的传感器,因此给AD421的数据的更新时间在5us,每次更新时DATA递增16,但是每圈有一个DATA由65536变成0的阶跃,请问这种情况下,AD421输出电流精度会有什么变化?
我使用了AD421。程序用三线模拟,硬件方面参考了中文规格书的电流源电路,其中没有用光耦,然后也没有用稳压源5V,电流输出LOOP RTN只接了一个1K的电阻出来。我使用的是外接电源5V给VCC,BOOST接VCC,VCC接4.7电解电容UF到地,LV接地,C1,C2,C3按规格书接了到COM,三根单片机的连线直接通过上拉10K 上拉到VCC接到STM32三根IO。
我试了修改程序,试了换芯片,试了查找相关资料,都没能解决如下问题:
不管我的DATA取什么值,我用万用表连接串有电阻的LOOP…
In addition, I would like to ask another question. In the datasheet of the AD5421, I find that the reference circuit of the AD5421 has been verified and registered as an approved HART solution by the HART Communication Foundation.Does the reference circuit…