• Offset Adjustment and Gain Adjustment

    Offset Adjustment and Gain Adjustment

     

    The gain adjustment range is fairly easy to calculate given other
    information on the data sheet, but the offset adjsut is more difficult
    without the internal schematics.

    Gain adjust: The 5k…
  • 关于AD420 电流一直输出4mA的问题。

    你好!

          一直使用的AD420总出现一些不稳定的问题,一直没有解决,现象是输出的电流一直是4mA,有时能正确输出。

  • AD420 4-20ma 输出时,12-20ma总是输出不对

    你好!

           我现在在调试AD420,0-65535输入,4-20ma输出,现在发现个问题,当我输入0-32767范围的时候,对应输出电流4-12ma,这是正确的,但是当我输入32768-65535这个范围的时候,电流输出也是4-12ma。而且当我输入65535的时候输出20ma。接线如下“

  • 请问使用AD420时配置输出0-24mA时,在有电流输出时芯片会发烫,是什么原因?电路如下:

  • RE: AD5422使用问题求教

    建议你可以参考附件的常见问题解答。

  • 变送器AD5412/22/10/20常见问题解答

    ADI中国技术支持团队精心整理了有关变送器AD5412/22/10/20的常见问题解答文档。想了解ADI专家们是如何解答以下常见问题吗?赶快下载文档吧!

     

    问题1 AD5420PIN 1451211均为GND,数字地和模拟地应该怎么区分?

    问题2 AD5420的评估板中的R27电阻的作用?

    问题3 AD5422EPAD脚如何处理,与什么连接呢

    问题4:在使用AD5422的过程中,选择0-5V输出范围,code=0000时,输出为0.027Vcode=FFFF时,输…

  • RE: AD420一直输出4mA

    AD421

    #include <stdio.h>

    #include <ADuC841.h>

    /*DEFINE CONTROL PINS OF ADUC841 FOR THE PURPOSE OF AD421 CONTROL.

    Customers should define the pins according to their design.*/

    sbit DATA=P3^3;

    sbit SCLOCK=P3^4;

    sbit LATCH=P3^5;

    void…

  • RE: AD421 Revision History

    Hi Manelous,

    AD420 is quite an old device - as you mention the datasheet revision of year 2000.

    For loop powered designs we are recommending AD5421 to be used in new designs.

    http://www.analog.com/en/digital-to-analog-converters/da-converters/ad5421…

  • RE: AD 420 interfacing with ATTiny 2313

    Hi,

    Apologies for the delay in repling to this query.

    Can you send on the digital waveforms that are being sent to this part?

    Also a brief description of the mode you wish to set the part up in would be useful.

    The AD5420 is the upgrade part to the…

  • RE: ADI 12位的adc 和DAC转换  有没有?

    对于ADC 12bit 8pin脚的产品,您可以考虑AD7893、AD7895(但是这两款都是外部参考);AD7896是内部参考。

    对于DAC产品,您可以考虑:AD420;AD5320和DAC8512。