FAQ
Hello,
I am interfacing Thermocouple K type with AD4110-1 ADC.
I got difference of 4 to 5 degree Celsius.
example: I set a temperature of 50 degree from calibrator, I got an output from ADC is 46 to 49 degree Celsius.
How to reduce noise?
is there any…
Hi Park,
1. yes, the internal clock is 8 MHz.
2. Please refer to the table 2 (timing specifications), figure 3 and Write Operation (pg 52) for better understanding of timing sequence.
3. As SYNC RESETs the device, it is recommended to wait 1ms as mentioned…
Hello,
I am interfacing two AD4110-1 devices on single SPI bus.
Reading of only one device works fine but getting unexpected reading when two device are reading in sequence.
Device 1 reading in RTD 4W mode,
ADC count of Device 1 = 5965 (only one device…
Hi,
I wants to convert output raw value of AD4110-1 into degree Celsius for RTD 4W sensor.
Can some one pls help me for how to convert raw value into temperature?
Thanks,
Jaydip
Dear Sir or Madam,
my name is Tristan Strahler and I am part of CURE Mannheim and we are currently evaluating the AD4110-1 AFE for usage in our new PLC systems. The analog functionality of the device exceeded our expectations so we opted to develop a…
Hi,
1. I am redirected to here from Precision ADC Q&A.
link to previous Q&A: (+) AD4110-1 MULTIPLE DEVICES ON THE SPI BUS - Q&A - Precision ADCs - EngineerZone (analog.com)
and also attached mail communication related to this issue.
2. Issue…
Dear Sirs
When I use AD4110-1 RTD function (excitation current).
May I use internal reference for RTD excitation current?
Or It must be to use external 2.5V reference?
BRS
Nat
Hello all,
I am facing issue in communicating with AD4110-1 via SPI pins in J2 connector on evaluation board using an external microcontroller. I am trying to read ID register as that register will be a static register hence it will be easy to know if…
Hi ADI Team,
Recently learnt about AD4110-1 and it seems to be a beautiful product with single chip solution for complicated AFE design.
I have one question thought, if we have to build a 18-channel Universal AFE then which analog switch is recommended to…