• RE: Missing LTspice files for AD4002

    Hi, 

    The model should be available within LTspice libraries. Please update your LTspice. The model can then be seen under ADC component list. 

    Thanks,

    Jellenie

  • RE: AD4002 SDO contention

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: PLL with External VCO, AD4002 and AD4110

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD7984

    Hi Roi,

    Thanks for your query. Unfortunately the answer is no, the AD7984 requires the input common mode voltage of the IN+ and IN- pins be nominally VREF/2. For example, if VREF = 5V, then the common mode voltage must be 2.5V at all times for the ADC…

  • RE: AD4003 negative output

    Thanks Rohit.

    You are using VREF = 5V, correct?

    If so, then the Common Mode Input Range specification is being violated and would explain why the output code is invalid.

    The common mode input range spec refers to the average voltage between IN+ and IN…

  • ADC 4002 simulation problem

    hi,

    when adding the ad4002 in ltspice i cant find which pins are the ones that appear in the datasheet.

  • too high "low" voltage level on GPIO

    Hi,

    I am trying to control ADF4002 by using EZKIT LITE 506F SPI1 controller and by using PG1 as latch enable.

    For some unclear reason, when the PG1 is cleared, it does not go below 440 mV which causes improper SPI latch enable.

    The code is attached…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…